How-to:
A USB flash drive with a maximum capacity of 8 GB, formatted in FAT32 and empty.

 
Instructions:
1. Open the ZIP file
2°- Copy the EVCS folder to the root of the USB drive
3°- Plug in the USB drive while the charging station is powered on
4°- Check the motherboard LED (at the back of the card slot); it should be flashing red.
5°- Wait 3 minutes
6°- The motherboard LED should be steady green
7°- Remove the USB drive